Synthesis of industrial design and functionality
Suitable for a broad spectrum of applications,
the new line was conceived for new market segments. These range from the construction
of hospital and medical equipment to laboratory fittings, from office furnishings to leisure and sporting equipment, and, generally, wherever aesthetics and user-friendliness are key requirements for the market success of a product.
 
A basic feature of the new elements, besides a perfect ergonomic function, is that of adding quality and value to the equipment for which they have been designed, by fully blending with it.

FIVE SMALL DOTS
  All products in the Ergostyle range are marked by five small dots.
They stand for the five letters in Elesa's name, an almost imperceptible signature, not to interfere with the brand identity of the product on which it fits.Be sure to look for them: a small, unobtrusive mark, making a world of difference.

ERGONOMIC DESIGN
We believe that good design should start
with a thorough understanding of
the product's functions.
In our case this means to take into account
the full set of movements involved in each operation of opening and closing, clamping, adjusting, setting or moving and evaluating
for each of them the interplay between man and machine taking place when the control element is being used.
These elements are not just simply designed to look good and provide a comfortable fit
for the hand, but are also meant to make life easier for the operator every time they are being used throughout the life-span of the object they have been designed for.
So, it is no real wonder that at its very first appearance Ergostyle obtained three
of the world most distinguished recognitions:
IF95
Die gute Industrieform
Hannover
Design 96 - Stoccarda
XVII Compasso d'Oro
Milano

Copyright © 2000 - 2006 Elesa.
Use of this site indicates your acceptance
of Terms of Use